VBUS.UVMODE

Description

VBUS.UVMODE sets what happens when the under voltage, UV, condition is detected. An under voltage is triggered:

When VBUS.UVMODE = 0, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH.

When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH and the controller attempts to enable the drive (software or hardware enable).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

VBUS.VALUE, VBUS.UVFTHRESH

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

VBUS.UVMODE

300ah

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.UVMODE

2512

9D0

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.UVMODE

2512

Unsigned8

Read/Write

-